Has anyone used mDDR with i.MX283?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has anyone used mDDR with i.MX283?

1,496 Views
JulieBirch
Contributor I

Hi!

I am wondering if anyone has been successful using mDDR instead of DDR2 with an i.MX283. The part I am using is MT46H64M16LF (Micron Tech). If anyone HAS been successful, I will have more questions for you!

 

Thanks!

Labels (1)
6 Replies

1,133 Views
dot_bob
Contributor I

You may have it working by now... I have mDDR (MT46H16M16LF) working with the i.MX28.  Let me know if you still have any questions.

 

-Rob

0 Kudos

1,133 Views
mp_baum_de
Contributor II

Hi Rob,

I want to use iMX287 with MT46H16M16LF (256MB, 4M*16*4 banks mobile LP DDR, 166MHz, 6.0 ns). Can you help me with the initialization routines?

Best regards,

Draghi

0 Kudos

1,133 Views
VladanJovanovic
NXP Employee
NXP Employee

Please see following page for init information:

https://community.freescale.com/docs/DOC-1455

1,133 Views
mp_baum_de
Contributor II

Hi Vladan,

thank you for the info. I was not able to download the file: MX28_DRAM_controller_register_programming_aid_v4.tar.gz

Can you give me a working link or simply send me the tool at mp_at_baum.de?

Best regards,

Draghi

0 Kudos

1,133 Views
VladanJovanovic
NXP Employee
NXP Employee

Attachments were missing on that page. Uploaded them to:

https://community.freescale.com/thread/300300

1,133 Views
mp_baum_de
Contributor II

Thanx a lot, Vladan!

0 Kudos