[HELP] surround view 3D 1.1 beta issue.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[HELP] surround view 3D 1.1 beta issue.

510 次查看
kangmw086
Contributor III

hi

i used IMX8QM-MEK.

I downloaded SURROUND VIEW 3D 1.1 beta.zip from the NXP site.

It is testing with reference to SVARM and SVAUG pdf documents.

i used YOCTO sumo-4.14.98.

And I also referred to the site below.

https://www.wpgdadatong.com/cn/blog/detail?BID=B0742

 

However, if you run the next software, it will stop as follows.

cd Tools/CamCapture/

./capturing 1

and keyboard 'p' press

Randomly dying. (1-10 times) --> segment fault.

 

----- error

sh-4.4# ./capturing 1
Width = 1280 Height = 800
Image size = 2048000
Pixelformat YUYV
WxH@fps = 1280x800@30 Image size = 2048000
Segmentation fault (core dumped)

 

In addition, even if captured, the stored image is as follows.

frame1_0.jpg

Do I need a patch?

 

regards.

 

 

0 项奖励
0 回复数