HELP NEEDED TO BUY OLD IMX6 SABRE EVAL KIT (IMX6SDL)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HELP NEEDED TO BUY OLD IMX6 SABRE EVAL KIT (IMX6SDL)

Jump to solution
545 Views
anirudhthabjul
Contributor I

Hello Everyone,

 

I am Anirudh THABJUL, Electronic engineer working in a company 'Second Bridge', We are situated in Paris.

 

We have designed our entire schematics from a sub contract company in 2012 using IMX6 SABRE DUAL LITE Eval kit.

 

Now we want to debugg some major issues.

 

So, In order to solve that issues with our present existing hardware we need the eval kit with reference IMX6SDL to debug the issues which is designed in 2009 to 2012 and is in obsolete condition now.

 

Please help me in finding it. It will be very helpful if some one have eval kit which is used (refurbished) also. We are ready to pay full fare if needed.

If possible suggest us some wesites where we can buy used eval kits.

 

Contact

 

PCBDesign@second-bridge.com

Thank you.

 

Regards,
Anirudh THABJUL

1 Solution
481 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Aniruth,

there might be a confusion. Please go to ARM Cortex-A9|i.MX 6 Multicore Processors|NXP  ( www.nxp.com/imx6 ). Here you will see al the IMX6 flavors and you will find i.MX 6 Solo Lite (i.MX6SL) and i.MX 6 Dual Lite (i.MX6DL) but there is no i.MX6SDL.

So, in order to buy you may click on the processor you are using and then click on the ´Software & Tools´ tab.

If you chose i.MX6SL look for i.MX 6SoloLite Evaluation Kit

If you chose i.MX6DL there are 2 options:

- SABBRE SD (Smart Devices) SABRE Platform for Smart Devices|NXP 

- SABRE AI (Automotive Infotaiment) SABRE|Automotive-Infotainment|i.MX6|NXP 

Once you select the correct device go to 'Buy / Parametrics' tab, here you can select to Buy direct or through a distributor.

I hope this helps.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
482 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Aniruth,

there might be a confusion. Please go to ARM Cortex-A9|i.MX 6 Multicore Processors|NXP  ( www.nxp.com/imx6 ). Here you will see al the IMX6 flavors and you will find i.MX 6 Solo Lite (i.MX6SL) and i.MX 6 Dual Lite (i.MX6DL) but there is no i.MX6SDL.

So, in order to buy you may click on the processor you are using and then click on the ´Software & Tools´ tab.

If you chose i.MX6SL look for i.MX 6SoloLite Evaluation Kit

If you chose i.MX6DL there are 2 options:

- SABBRE SD (Smart Devices) SABRE Platform for Smart Devices|NXP 

- SABRE AI (Automotive Infotaiment) SABRE|Automotive-Infotainment|i.MX6|NXP 

Once you select the correct device go to 'Buy / Parametrics' tab, here you can select to Buy direct or through a distributor.

I hope this helps.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------