HDMI output in I.MX6QPLUS SabreSD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI output in I.MX6QPLUS SabreSD

985 Views
jdepedro
Contributor IV

I am trying to get HDMI output using the following imageS:

MACHINE=imx6qpsabresd source fsl-setup-release.sh -b imx6qp-workspace/

bitbake fsl-image-qt5

Do I need to configure from U-Boot? 

0 Kudos
Reply
1 Reply

870 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jose

for hdmi please refer to Table 10. Common kernel boot parameters p.19

attached Release Notes and sect.4.3.2 Copying the full SD card image

Linux Guide. Use Demo Images on

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&location=null&Pa... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply