HDMI drive strength control and pixel clock change

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HDMI drive strength control and pixel clock change

2,111 次查看
ani10c89
Contributor II

Hi,

We are facing issues with HDMI port during EMI test. Can you please let us know documentation to change the drive strength and pixel clock for HDMI interface.

Regards,

Anirudha

标签 (1)
0 项奖励
回复
6 回复数

1,850 次查看
b36401
NXP Employee
NXP Employee

Actually pixel clock depends of FPS and the resolution. Please refer to table 15-6 of i.MX8M Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

As for drive strength it can be changed with HDMI firmware.
Please refer to section 6.1.6.2 "HDMI image boot up" of the Reference Manual for the details.
However it is not supported with our BSP.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,850 次查看
ani10c89
Contributor II

Hi Victor,

Can you please help to change the drive strength in BSP. Please provide the documentation on how HDMI booting can be enabled in BSP.

This is very critical to resolve the HDMI EMI issues.

Regards,

Anirudha

0 项奖励
回复

1,850 次查看
b36401
NXP Employee
NXP Employee

The drive strength can not be changed in BSP. You need to update HDMI firmware.

0 项奖励
回复

1,850 次查看
sandeep_yenugul
Contributor III

Hi Victor,

I have got a binary of HDMI firmware in imx-boot/0.2-r0/git/iMX8M/signed_hdmi_imx8m.bin. But from where can I get source code for same so that I can edit the drive-strength in it, recompile and test it.

0 项奖励
回复

1,850 次查看
ani10c89
Contributor II

Can you provide details or documentation for it which can help us control the drive strength.

Can you please provide the support for this as it is critical for EMI testing.

Regards,

Anirudha

0 项奖励
回复

1,850 次查看
ani10c89
Contributor II

Hi,

Any update.

Regards,

Anirudha

0 项奖励
回复