HD:1080*720 display normally based on IMX6D6AVT10AE @ Android 4.2.2(L3.0.35)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HD:1080*720 display normally based on IMX6D6AVT10AE @ Android 4.2.2(L3.0.35)

928件の閲覧回数
john_li2
Contributor I

Dears,

Performance test needed, and display anormally when transfer the OS from Linux 3.0.35 to Andriod 4.2.2(based on L3.0.35). Could you help to check and suggest if we need to display in HD:1080*720, thanks.

CPU: MCIMX6D6AVT10AE + TP9950

OS: Linux 3.0.35

Testing: (1ch * camera) 

Display definition: 720*576, Result: Display normally, OK;

Display definition: 1080*720, Result: Display normally, OK;

OS: Android 4.2.2 (L3.0.35) 

Testing: (1ch * camera) 

Display definition: 720*576, Result: Display normally, OK;

Display definition: 1080*720, Result: Display abnormally, NG; and the picture as attached file.

0 件の賞賛
返信
3 返答(返信)

923件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @john_li2 ,

 

The version of android and Linux that you are using are no longer supported from our part, you should try our newer versions of android and Linux (Andriod 10 and L5.4.47_2.2.0), that you can find on the link below, your issue probably get fix on the newest versions.

https://www.nxp.com/design/software/embedded-software/i-mx-software:IMX-SW

 

Regards,

Israel H.

0 件の賞賛
返信

896件の閲覧回数
john_li2
Contributor I

Dear Israel,

Thanks very much for your reply, version transfer is a big work for ourside, and we had try to solve the problem based on Android4.2.2. these weeks, but no any process.

Could you tell us the root reason of the issue?

Is there any opportunity if we would try to solve the probolem based on current version?

If yes, any suggestion, please let me know, thanks.

0 件の賞賛
返信

917件の閲覧回数
john_li2
Contributor I

Hi,

Got it, will check and try, thanks.

0 件の賞賛
返信