H.264 sample video

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,161件の閲覧回数
tetsuomaeda
Contributor III

Hi,

This is my first question at this forum.

We are thinking to use iMX6 series for our H.264 video encoding platform.

The target bit rate is 14Mbps at 1920 x 1080p resolution.

1. Are there any sample encoded video that can be used for our evaluation?

2. Is there a software encoder which emulates the quality of the iMX6 H/W encoder?

.

Thanks in advance for the information.

Tetsuo.

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
930件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi TETSUO

I am afraid there are no such samples or test apps.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
931件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi TETSUO

I am afraid there are no such samples or test apps.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
930件の閲覧回数
tetsuomaeda
Contributor III

Hi Igor-san,

Thank you for the reply.

I'll look for other method.

Regards,

Tetsuo

0 件の賞賛
返信