GST_DEBUG="*:2" gst-launch-1.0 -v -e multifilesrc location="image%05d.png" index=0 stop-index=3 caps="image/png,width=960,height=540,framerate=1/1" ! \ pngdec ! queue ! videoconvert ! imxvpuenc_h264 ! h264parse ! mp4mux ! filesink location=images.mp4
Setting pipeline to PAUSED ... Pipeline is PREROLLING ... 0:00:00.189972820 26707 0x12f0380 WARN basesrc gstbasesrc.c:2943:gst_base_src_loop:<multifilesrc0> error: Internal data flow error. 0:00:00.190759558 26707 0x12f0380 WARN basesrc gstbasesrc.c:2943:gst_base_src_loop:<multifilesrc0> error: streaming task paused, reason not-negotiated (-4) ERROR: from element /GstPipeline:pipeline0/GstMultiFileSrc:multifilesrc0: Internal data flow error. Additional debug info: /path/to/yocto_guf/build-imx6guf/tmp/work/cortexa9hf-vfp-neon-guf-linux-gnueabi/gstreamer1.0/1.6.0-r0/gstreamer-1.6.0/libs/gst/base/gstbasesrc.c(2943): gst_base_src_loop (): /GstPipeline:pipeline0/GstMultiFileSrc:multifilesrc0: streaming task paused, reason not-negotiated (-4) ERROR: pipeline doesn't want to preroll. Setting pipeline to NULL ... Freeing pipeline ...
gst-launch-1.0 -v -e multifilesrc location="image%05d.png" index=0 stop-index=3 caps="image/png,width=960,height=540,framerate=1/1" ! \ pngdec ! queue ! videoconvert ! filesink location=foo
gst-launch-1.0 videotestsrc num-buffers=1 ! imxvpuenc_h264 ! h264parse ! mp4mux ! filesink location=i.mp4
Pipeline is PREROLLING ... 0:00:00.263635740 29136 0xd931b0 INFO GST_ELEMENT_PADS gstelement.c:894:gst_element_get_static_pad: no such pad 'sink' in element "multifilesrc0" 0:00:00.264714837 29136 0xd931b0 FIXME default gstutils.c:3766:gst_pad_create_stream_id_internal:<multifilesrc0:src> Creating random stream-id, consider implementing a deterministic way of creating a stream-id 0:00:00.265199547 29136 0xd931b0 FIXME videodecoder gstvideodecoder.c:1057:gst_video_decoder_drain_out:<pngdec0> Sub-class should implement drain() 0:00:00.267156057 29136 0xd931b0 WARN basesrc gstbasesrc.c:2943:gst_base_src_loop:<multifilesrc0> error: Internal data flow error. 0:00:00.267523090 29136 0xd931b0 WARN basesrc gstbasesrc.c:2943:gst_base_src_loop:<multifilesrc0> error: streaming task paused, reason not-negotiated (-4) 0:00:00.267856120 29136 0xd931b0 INFO GST_ERROR_SYSTEM gstelement.c:1837:gst_element_message_full:<multifilesrc0> posting message: Internal data flow error.
Solved! Go to Solution.
Thanks for your reply. I could fix this, the error was the invalid image height (540, not a multiple of 8).
Anyway, the working (and cleaned-up; videoconvert is redundant, as well as mp4mux) pipeline now reads:
GST_DEBUG="*:2" gst-launch-1.0 -v -e multifilesrc location="image%05d.png" index=0 stop-index=3 caps="image/png,width=960,height=540,framerate=1/1" ! \ pngdec ! 'video/x-raw,format=i420' ! \ imxvpuenc_h264 ! filesink location=images.mp4
Thanks for your reply. I could fix this, the error was the invalid image height (540, not a multiple of 8).
Anyway, the working (and cleaned-up; videoconvert is redundant, as well as mp4mux) pipeline now reads:
GST_DEBUG="*:2" gst-launch-1.0 -v -e multifilesrc location="image%05d.png" index=0 stop-index=3 caps="image/png,width=960,height=540,framerate=1/1" ! \ pngdec ! 'video/x-raw,format=i420' ! \ imxvpuenc_h264 ! filesink location=images.mp4
HI Aleph
gstreamer-imx is used on the case, which is not supported by nxp,
please check maintainer of gstreamer-imx plugins mentioned on
https://community.nxp.com/thread/445732
Alternatively one can try nxp nxp gstreamer plugins described in Linux Guide
in documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------