Graphic accelerated browsing on IMX6 using QWebkit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Graphic accelerated browsing on IMX6 using QWebkit

916 Views
christianeissle
Contributor I

Hi Communitiy,

I tried to build an graphic accelerated browser on a Wayland rootfs based on the Yocto (daisy) release.

I currently have a working rootfs with Wayland(weston compositor), Qt, Qtwayland plugin and Qwebkit integrated. I created a small QwebView browser which is working successfully with HTML5 and Javascript content but doesn't using hardware acceleration.

It is possible to create OpenGL application with QML and the wayland-egl plugin and also QWidget based applications so that it is sure that OpenGL support is available for Wayland.

Using a QGraphicsWebView or a accelerated QML WebView doesn't work.

Does anyone have expieriences using hardware accelerated browsing with th IMX6 using QWebkit? I'm using the Nitrogen6x board from BoundaryDevices

Regards Christian Eissler

Labels (1)
0 Kudos
Reply
0 Replies