Hi all,
I am using the imx7ulp board for my project . I am using yoct os . I have to know the gpu performance while rendering or capturing the image. I observed while rendering the image , the logs present in the code was used it under os/linux/drivers/gpu/drm/etnaviv that means my gpu using the ethnaviv driver instead of galcore driver. could you please help me in meausring the performance of gpu which is using the ethnaviv driver for rendering.
I have the following info
Operating System: Poky (Yocto Project Reference Distro) 2.7.1 (warrior)
Kernel: Linux 4.14.98
uname -a Linux fly 4.14.98
#1 SMP PREEMPT Mon Jul 10 16:01:38 UTC 2023
armv7l GNU/Linux build/yocto/poky/meta-yocto-bsp/conf : file content
# We have a conf and classes directory, add to
BBPATH BBPATH .= ":${LAYERDIR}" # We have recipes-* directories,
add to BBFILES BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \ ${LAYERDIR}/recipes-*/*/*.bbappend"
BBFILE_COLLECTIONS += "yoctobsp" BBFILE_PATTERN_yoctobsp = "^${LAYERDIR}/"
BBFILE_PRIORITY_yoctobsp = "5"
LAYERVERSION_yoctobsp = "4"
LAYERSERIES_COMPAT_yoctobsp = "warrior"
You are using the ethnaviv driver not the GPU driver we using, so we do not have test the performance for this driver.
If you want to use the GPU of NXP, you can modify in the Menuconfig.
You can refer to our i.MX_Graphics_User's_Guide.pdf document.
In menu configuration enable the following module for the GPU driver:
CONFIG_MXC_GPU_VIV is a configuration option for GPU driver. In the menuconfig this option is available under Device Drivers
> MXC support drivers > MXC Vivante GPU support > MXC Vivante GPU support.
On the screen displayed, select Configure the kernel, select Device Drivers > MXC support drivers > MXC Vivante GPU support
> MXC Vivante GPU support, and then exit. When the next screen appears, select the following options to enable the GPU driver:
• Package list > imx-gpu-viv
• This package provides proprietary binary libraries, and test code built from the GPU for framebuffer