Hi,
I want to change the gplay(gst-fsl-plugin-2.0.3) video screen size with 700x300. I have modified the file mfw_gplay_core.c with the below changes.
#define DEFAULT_OFFSET_X 65
#define DEFAULT_OFFSET_Y 100
#define DEFAULT_DISPLAY_WIDTH 700
#define DEFAULT_DISPLAY_HEIGHT 300
But these changes also not taking into the effect and the video screen size remains same. Could you kindly help in fixing this issue
Regards,
Swamy
Thanks for the reply.
Strangely fsl_player_full_screen() function is not getting called from anywhere. I even added forcefully the following parameters under the function fsl_player_play(), but still no change in the display area. It is still occupying the entire display resolution. Please suggest.
pproperty->display_parameter.offsetx = DEFAULT_OFFSET_X; | |
pproperty->display_parameter.offsety = DEFAULT_OFFSET_Y; | |
pproperty->display_parameter.disp_width = DEFAULT_DISPLAY_WIDTH; | |
pproperty->display_parameter.disp_height = DEFAULT_DISPLAY_HEIGHT; | |
pproperty->bfullscreen=0; //added |
pplayer->klass->resize(pplayer, pproperty->display_parameter);
Regards,
Swamy
Mahadeva, what is the progress of your issue? If your issue had been resolved please click Correct Answer/Helpful Answer. We would liek to close your DI if no response from you in 3 days.
Thanks,
Yixing
Hi.
Could you, please, let me know the status of this issue?
I think missed the notification of your update.
Please, take a look on fsl_player_ret_val fsl_player_full_screen(fsl_player_handle handle) in order to determinate value of pproperty->bfullscreen
I believe gplay is configured for fullscreen by default.