Hello,
A few years ago we designed a system based on the IMX6 processor. Voltages for this design are controlled by a PMIC (PF0100NPEP up to now). The PMIC configuration is done through an I²C interface (thanks to a programmed microcontroller). This system was used in the past years.
We are now manufacturing new cards with the new PMIC version (PF0100NPAEP), the previous one being obsolete. These new PCBs work nicely but for an issue during booting. When booting we observe two different behaviors:
- If the card was not recently (recently is a maximum of around 4 seconds) plugged in, the card will not boot.
- If the card was plugged recently, the card will boot.
By observing different signals on the card during power-up we deduced that PMIC is in cause. More precisely signal VSNVS (and associated PWRON) do not behave correctly.
The associated circuitry (or the rest of the PCB) should not be in cause since we were able to obtain good results by changing the NPAEP back to NPEP on one of the new cards.
The program used in the PIC to configure PMIC (by I²C) was not modified during the tests.
Recordings of the measured VSNVS signal are in attachment in three different cases:
- When PCB is not booting (with NPAEP version): signal takes the wanted value (3V) for a short time and then goes back to 1V.
- When PCB is booting (with NPAEP version): we see an unwanted step at around 2.6V but the final value is what is expected.
- When (new) PCB is booting with an old NPEP version we still had in stock. We were able to replace NPAEP with NPEP version. This card behaves as expected.
We were not able when going through the PMIC datasheet and errata to find what change which occurred between NPEP and NPAEP version could cause this type of behavior.
Would you have any idea of what could cause this behavior ? Any idea on what we could do to solve this ?
Thanks
Camille
Hi Camille
VSNVS signal at 1V may be caused by floating LICELL, so
recommended to connect LICELL pin to VIN or use valid coincell. Behaviour
is described in sect.6.4.7 VSNVS LDO/switch MMPF0100 datasheet
http://www.nxp.com/assets/documents/data/en/data-sheets/MMPF0100.pdf
Workarounds described in errata for old version are not needed for MMPF0100A.
http://cache.freescale.com/files/analog/doc/errata/MMPF0100ER.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Thank you for your answer.
For what regards LICELL pin I double checked the circuit. We indeed had a small problem here.
This one is solved now and the different steps taken by VSNVS do not appear anymore (we go directly from 0 to 3V when we boot correctly).
However PCB still sometimes doesn't boot (same behavior as before) and VSNVS net still takes the weird shape when we do not boot (NPAEP_no_boot.jpg of my initial post).
I've already checked workarounds which are not applicable and none of them are implement on our PCB.
Any over clue ?
We are now suspecting a timing error during power up/configuration (linked to software on the associated PIC). Any idea in this direction ? Do you know if some timings changed between versions ?
Again, thank you,
Regards,
Camille
Hi Igor,
I can now confirm that VSNVS goes directly to 3V.
In the mean time we found our mistake. Errata number 19 was taken care of in a different way as mentioned in the errata document. I missed it before. When this workaround is removed, we don't have anymore problem.
Everything work nicely for this card.
I will go threw our other designs using PMIC now.
Again, thank you for your answers.
Best regards,
Camille