Get YOCTO on the i.MX6 + MCIMX-LVDS1 screen + Qt 4.8/5.1 Multitouch working?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Get YOCTO on the i.MX6 + MCIMX-LVDS1 screen + Qt 4.8/5.1 Multitouch working?

738件の閲覧回数
florianl
Contributor III

Hello everybody!

Did anyone of you get the Multitouch of the MCIMX-LVDS1 running with a YOCTO build and an Qt 4.8 or 5.1 application?

It seems like the multitouch is already working on the device because it generates multiple outputs in evtest on touching the device with multiple fingers.

But in my Qt 4.8 Application the cursor only jumps between my two fingers while I touch the screen with two fingers. More than two fingers are not recognized by the application.

Any suggestions?

Best regards

Florian

ラベル(4)
0 件の賞賛
返信
0 返答(返信)