Generic data format of i.mx6 IPU CSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generic data format of i.mx6 IPU CSI

941 Views
宗標廖
Contributor V

Hello, Community

I asked a question at https://community.nxp.com/message/667685?et=watches.email.thread#comment-667685.

But igorpadykov 従業員 let me to start a new thread.

In my use case, the MIPI camera sensor output data of RGB666 format. But according to register of IPUx_CSI0_SENS_CONF in IMX6DQRM(Rev.3),it looks like that the IPU CSI of i.mx6 cannot receive RGB666 data.

pastedImage_0.png

igorpadykov 従業員 suggests me to handle RGB666 data as generic format.

About generic format, I have two questions.

Q1)

If set CSI0_SENS_DATA_FORMAT to generic data, then how to set CSI0_DATA_WIDTH?

153350_153350.pngpastedImage_4.png

Q2)

If RGB666 input is received as generic data ,then how to resolve it back to RGB666 format(Need I write some custom code)?

Thank you!

ZongbiaoLiao

Labels (5)
0 Kudos
2 Replies

460 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

please look at below links they explain these questions

MX53 CSI/IDMAC config for Aptina 12-bit graysca... | NXP Community

https://community.freescale.com/message/344529#344529

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

460 Views
宗標廖
Contributor V

Hi Igor

Thank you for you reply!

I found what I want in i.MX6 OV5647 Bayer sensor driver (ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0)

In IMX6DQRM, there is description as bellow:

-----------------------------------

37.4.3.2.2

High-speed serial interface - MIPI (Mobile Industry Processor

Interface).

In MIPI interface two values arrive in each cycle. Each value is 8 bit wide, which means

16 MSB bits of the data bus input are treated, while 4 LSB bits are ignored.

When working in this mode, the CSI can handle up to 4 streams of data. Each stream is

identified with DI (data identifier) that includes the virtual channel and the data type of

this stream. Each stream that is handled is defined in registers MIPI_DI0-3. Only the

main stream (MIPI_DI0) can be sent to all destination units while the other streams are

sent only to the SMFC as generic data.

In this mode SENS_DATA_FORMAT and DATA_WIDTH registers are ignored, since

this information is coming to the CSI via the MCT_DI bus.

-----------------------------------

Thank you!

ZongbiaoLiao

0 Kudos