Generic SPIFI flash driver for iMXRT1020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generic SPIFI flash driver for iMXRT1020

Jump to solution
2,155 Views
tomsong
Contributor III

Hi,

     I can't find a generic SPIFI flash driver file for iMXRT1020. Is it included with the MCUXpresso?

    Thanks!

1 Solution
1,540 Views
lpcxpresso_supp
NXP Employee
NXP Employee

MCUXpresso IDE v10.2.1 now provides a self configuring LinkServer QSPI flash driver. For more details, please see: https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2018/07/27/mcuxpresso-ide-v1021-n... 

Regards,

MCUXpresso IDE Support

View solution in original post

6 Replies
1,541 Views
lpcxpresso_supp
NXP Employee
NXP Employee

MCUXpresso IDE v10.2.1 now provides a self configuring LinkServer QSPI flash driver. For more details, please see: https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2018/07/27/mcuxpresso-ide-v1021-n... 

Regards,

MCUXpresso IDE Support

1,540 Views
tomsong
Contributor III

I download the new MCUXpresso and found the flash driver.

0 Kudos
Reply
1,540 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tom

please check p.121 attached MCUXpresso document describing processors with support for SFDP.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,540 Views
tomsong
Contributor III

Hi Igor,

     It is not listed in the document. It mentioned "Drivers for other MCUs supporting external QSPI may be made available post release". So I wonder is the driver for iMXRT1020 available? If not how can I write my own driver?

    Thanks!

     Regards,

     Tom

0 Kudos
Reply
1,540 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tom

 

provided document described supported platforms for SFDP. Seems newer MCUxpresso v10.2.1 supports

SFDP  for iMXRT1020 as described below from LPCX presso support:

pastedImage_1.jpg

Best regards
igor

1,540 Views
tomsong
Contributor III

Hi Igor,

     Thanks! The new version of MCUXpresso has the driver.

0 Kudos
Reply