Generating a pulse with M4 Core on Imx8 Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generating a pulse with M4 Core on Imx8 Mini

1,659 Views
Alirezah95
Contributor II

Hi.

I'm trying to generate a pulse on a GPIO pin using M4 Core and I have built the M4 firmware for this purpose too and the pulse is being generated successfuly (I'm using uboot to load the firmware). Everything works as expected unitl the kernel boots up and then the pulse vanishes in the osciloscope. I've checked and confirmed that the code is still running correctly on the M4 core but it looks like the kernel has taken the ownership of GPIO, so the M4 core is not able to actually change the pin value. Is that right? If so how would I fix this? How would I prevent kernel from taking the ownership of GPIO so the pulses keep generating even after kernel boots up.

Labels (1)
0 Kudos
Reply
2 Replies

1,622 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

M4 is low power microcontroller available for customer application:
• Low power standby mode
• IoT features
• Manage IR or wireless remote

Also one can look at below app notes describing M4 usage:

AN12225 How to Reduce SoC Power when Running M4 with A53 on i.MX8M
AN12195 Implement Low-Power Audio on i.MX8M

 

Regards

0 Kudos
Reply

1,617 Views
Alirezah95
Contributor II
So is it possible to generate pulses using m4 while the os is running?
0 Kudos
Reply