Hi,
Is the i.MX6Q capable of doing 16 display (4 x 4) using gstreamer?
I've seen the following example for ( 2 x 2 ) is that the limit?
https://community.freescale.com/docs/DOC-93788
Thanks,
Tarek
解決済! 解決策の投稿を見る。
to solve this problem gst-fsl-plugins package should be modified as follow:
In file: mfw_gst_vss_common.c change vd->vsmax = 4 to vd->vsmax = 16
In file: mfw_gst_vss_common.h change #define VS_MAX 8 to VS_MAX 16
Re-build and deploy!
That's it.
to solve this problem gst-fsl-plugins package should be modified as follow:
In file: mfw_gst_vss_common.c change vd->vsmax = 4 to vd->vsmax = 16
In file: mfw_gst_vss_common.h change #define VS_MAX 8 to VS_MAX 16
Re-build and deploy!
That's it.