GPU accelerated browser

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPU accelerated browser

799 Views
bharadwaaj
Contributor III

Hi all,

   I have a graphic intensive application which has to be run on the browser in kiosk mode in linux. So far tested with crhomium in i.MX6 dl sabreauto. Please let me know which browser supports GPU acceleration and do i need to do any configurations for the same.

Thanks in advance...

Tags (3)
0 Kudos
1 Reply

529 Views
igorpadykov
NXP Employee
NXP Employee

HI Bharadwaaj

for browsers please look at attached Yocto Guide from L3.14.28_1.0.0_iMX6QDLS_BUNDLE

sect.5.6.6 Chromium Browser on X11 and Wayland

sect.5.6.7 Qt5 and WebKit browser

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos