GPU (Galcore.ko) is not working on .mx6-SOLOsabresd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPU (Galcore.ko) is not working on .mx6-SOLOsabresd

1,171件の閲覧回数
noammoshe
Contributor II

In one of our boards we use i.mx6-SOLOsabresd  (MCIMX6S5EVM10AC) with Embedded Linux. Our current versions are:

  •       Kernel 4.1.15
  •       Jethro (Yocto version 2.0)

 

In order to apply a certain feature we need to upgrade the BSP (Kernel, Linux,..). We tried:

  •       Sumo (Yocto version 2.5) version with kernel 4.14
  •       Rocko (Yocto version 2.4) version with kernel 4.9
  •       Rocko (Yocto version 2.4) version with kernel 4.9.88 (specific version)

 

Using the next images:

 

In all of the cases we encountered with the same problem – the GPU (Galcore.ko) is not working, we cannot run our graphic apps.

 

We need a solution for i.mx6-SOLOsabresd (MCIMX6S5EVM10AC).

 

Notes

タグ(1)
0 件の賞賛
2 返答(返信)

935件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Noam,

For galcore you need to run the 5.0.11 version of the vivante driver and kernel 4.1.15, this don´t work for newer BSPs because NXP doesn´t  have the MX6SoloSabreSD.

Regards

0 件の賞賛

935件の閲覧回数
noammoshe
Contributor II

Dear Bio_TICFSL Employee

For galcore you need to run the 5.0.11 version of the vivante driver and kernel 4.1.15

In order to apply certain things I need an updated BSP, the current version (4.1.15) does not help me.

NXP doesn´t  have the MX6SoloSabreSD.

What does it means?

0 件の賞賛