Hello,
I Want To Read/Write Data Direct GPIO Pin A Pind address Through Device Driver And I Want to Change GPIO Pin Address So, Can You Explain Which Driver File I Need Change ? And How to I Change GPIO Pin Address?
ok. hi nirjul how r u
2 for imx8 i will told you no have much SPARE GPIO pins for us to use , all of them are reused for others , u must undestand this
3
for imx 8 we normal do LInux , open file , operate file to operate the port , not bare metal
4
base on this , you can read the board reference manual , not short one , but some 9111 pages references manual one
to find what port u can use lah
5
see my project << how to port imx8 gpio in linux bsp l5.10.35...>>
i find our this pcieb not in use , no have wifi moudle for my board si b0 , so can modified the circuits then port to LEDS
==========================================================
of cause have lah; in line 1406# of file imx8x.dtsi
pinctrl_pcieb: pcieagrp{
fsl,pins = <
IMX8QXP_PCIE_CTRL0_PERST_B_LSIO_GPIO4_IO00 0x06000021
IMX8QXP_PCIE_CTRL0_CLKREQ_B_LSIO_GPIO4_IO01 0x06000021
IMX8QXP_PCIE_CTRL0_WAKE_B_LSIO_GPIO4_IO02 0x04000021
>;
};
thank you as you helps r great !!! i accepted it as a solution , thank you again
============================================================
6 thank you , hope you can find out the correct way and enjoy developing .
joseph
ok. hi nirjul how r u
2 for imx8 i will told you no have much SPARE GPIO pins for us to use , all of them are reused for others , fews gpio can be exported
root@imx8qxpmek:/sys/class/gpio# ls
export gpiochip128 gpiochip224 gpiochip472 gpiochip96
gpio32 gpiochip160 gpiochip32 gpiochip480 unexport
gpiochip0 gpiochip192 gpiochip464 gpiochip64
root@imx8qxpmek:/sys/class/gpio#
even no have any User LEDs all r system LEDs such as numlock/ caps lock and scrolllock , all under system control , u must undestand this. if u really interest in operate gpio pins , u might try Arduino Uno or TI MSP430 . many gpio there r open for user to control
3
for imx 8 we normal do LInux , open file , operate file to operate the port , not bare metal
(even in bare metal we all fellow the system defines the address of any port and pins , to let your program more readable and portable lah)
4
base on this , you can read the proceesor and board reference manual , not short one , but some50mb pdf file and about 9111 pages references manual one(for my board imx8qxpmek , yours also about 6000pages if i m not wrong), to read every things insides and
to find what port u can use lah
5
see my project << how to port imx8 gpio_LED in linux bsp l5.10.35...>>here the link:
i also only just find out this pcieb pin not in use , no have wifi moudle for my board si b0 , so can modified the circuits then port to LEDS
============================finally done it==============================
of cause have lah; in line 1406# of file imx8x.dtsi
pinctrl_pcieb: pcieagrp{
fsl,pins = <
IMX8QXP_PCIE_CTRL0_PERST_B_LSIO_GPIO4_IO00 0x06000021 // dun chge this address pls
IMX8QXP_PCIE_CTRL0_CLKREQ_B_LSIO_GPIO4_IO01 0x06000021
IMX8QXP_PCIE_CTRL0_WAKE_B_LSIO_GPIO4_IO02 0x04000021
>;
};
thank you as you helps r great !!! i accepted it as a solution , thank you again
============================================================
6
u no need to channged the default port / pin address and dun do so , it is always the same address say
IMX8QXP_PCIE_CTRL0_PERST_B_LSIO_GPIO4_IO00 0x06000021 // dun chge this address pls
thank you , hope you can find out the correct way and enjoy developing .
@Nirjul_Patel
Hello,
i.MX8 device tree files are located in
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale?h=lf-5.10.y
The DTS files include .h files with pins definitions.
Use pinctrl binding documents in Documentation/devicetree/bindings/pinctrl/fsl.
Also: imx8??-pinfunc.h under device tree source folder.
Regards,
Yuri.
Hello,
Thanks For Your Quickly Supoort
I Use i.MX8mm-ddr4-evk board And I Built imx-image-multimedia So,
How to Get Particular GPIO Pin Address?
Which Pin Available Convert to GPIO Pin?
How to Read/Write Data Direct GPIO Pin Address?