GPIO in i.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO in i.MX6UL

877 次查看
anshulkhare
Contributor III

Hello All,

My platform is i.mx6ul, i have enabled the GPIO driver in menu configuration.but it is not visible in

/dev/gpio file system.

 

If I look at /sys/class/gpio on my card, I am able to find the gpio file system

 

 Could any one help me to solve this issue?

标签 (1)
标记 (3)
0 项奖励
2 回复数

609 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Anshul

please look at example on

Simple GPIO Example - quandry 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

609 次查看
anshulkhare
Contributor III

Hello igor,

            Thank you for reply , i am able to set the direction of gpio pins and i am performing read and write operation,

            in path like sys/class/gpio/gpioN/ .but iam not getting gpio in the /dev file system like /dev/gpio.

    

Best Regards

Anshul

0 项奖励