Freeze Low Power Mode is not working with i.MX6 SoloLite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freeze Low Power Mode is not working with i.MX6 SoloLite

1,089 Views
vipulkumar
Contributor III

Hi,

I am using customized i.MX6 SL board with TPS65910 PMIC. I am able to wakeup the board from the STANDBY low power mode by using TPS65910 PMIC rtc but failed to wakeup the from the FREEZE low power mode.

OS - Linux

Kernel - 3.14

Yocto - 2.0

Procedure:

date -s "2016-07-20 11:03:59"

hwclock --systohc

echo +40 > /sys/class/rtc/rtc0/wakealarm

cat /proc/driver/rtc

rtc_time    : 11:05:30
rtc_date    : 2016-07-20
alrm_time   : 11:06:05
alrm_date   : 2016-07-20
alarm_IRQ   : yes
alrm_pending: no
update IRQ enabled  : no
periodic IRQ enabled: no

periodic IRQ frequency  : 1

max user IRQ frequency  : 64

24hr        : yes

echo freeze > /sys/power/state

PM: Syncing filesystems ...

done.

Freezing user space processes ... (elapsed 0.010 seconds) done.

Freezing remaining freezable tasks ... (elapsed 0.005 seconds) done.

Suspending console(s) (use no_console_suspend to debug)

Labels (4)
0 Kudos
1 Reply

623 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vipul

"Freeze" low power mode is not supported in i.MX6 nxp

bsp releases, please refer to attached Linux Manual

Chapter 22 Low-level Power Management (PM) Driver

for supported modes. One can try them using nxp bsp on

linux-2.6-imx.git - Freescale i.MX Linux Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos