Video property is as follows :
Topology:
container: Audio Video Interleave (AVI)
audio: MPEG-1 Layer 3 (MP3)
video: ITU H.264
Properties:
Duration: 1:03:59.059562500
Seekable: yes
Tags:
video codec: ITU H.264
audio codec: MPEG-1 layer 3
encoder: MEncoder SVN-r29352(20090610-gcc4.3.3)
container format: AVI
nominal bitrate: 128000
has crc: false
channel mode: joint-stereo
bitrate: 128000
We are using aiurdemux, vpudec and mfw_v4lsink.
Our Pipeline
gst-launch=0.10 filesrc location=/mnt/usb/Visteon_800_480_1.avi typefind=true !
aiurdemux name=demux demux. ! queue ! vpudec ! mfw_v4lsink demux. ! queue !
beepdec ! audioconvert ! alsasink
It is not reproducing always. On repeated playback we observed sometimes.
We have observed same behavior with playbin2 also.
File size is too big, So not able to attach here. If required we will upload file in FTP.
We are using gst-fsl-plugins version 3.5.7 and gstreamer version 10.36
Result of "uname -a" is
Linux freescale 3.0.35-2154-g94689e1 #180 SMP PREEMPT Wed Mar 4 15:24:49
CST 2015 armv7l GNU/Linux
BSP version is 3.0.35 based customized BSP.
Board is IM6D based customized board .
This is very urgent, for a production program. SOP is very close.
Please help us analysing this ASAP.
Regards:
Ramakrishna Kamath
Hi,
I have consulted with the experts, and it would be required the specific file and configuration that you have used. Additionally, it could be better if there is available an “always reproducible” procedure. Did you was able to upload file to any other server?
Best regards!
/Carlos
Hi Carlos,
Currently we don't know, how to reproduce this issue always.
We are able to reproduce with playbin. So it is not related to our configuration.
Only steps we knew to reproduce is playing video with playbin.
If it plays fine, stop and retry to play.
We have uploaded log and file in Our FTP server at path: "/data/From_Allgo_To_FSL/354686/Frame Drop in Vpudec .tar.bz2"
HI jackmao
Please help Carlos to get file from FTP.
Thanks and Regards,
Ramakrishna Kamath