Fow what value i can set as following TBD, in MX8M_LPDDR4_RPA_v24.xlsx file ,when I want set 1866MHZ,thanks and best regards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fow what value i can set as following TBD, in MX8M_LPDDR4_RPA_v24.xlsx file ,when I want set 1866MHZ,thanks and best regards

542件の閲覧回数
jw216
Contributor I

Fow what value i can set as following TBD, in MX8M_LPDDR4_RPA_v24.xlsx file ,when I want set 1866MHZ,thanks and best regards

memory set0x3036006832TBD#HW_DRAM_PLL_CFG2_ADDR: For 1866MHz DDR speed, Configure DRAM PLL for 933MHz operation
0 件の賞賛
1 返信

476件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi charles

in general "TBD" values can be left in default state.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛