Hello all,
How do I add the Freescale FlexCAN driver (All Boards FlexCAN ) to the latest android kernel from freescale (n7.1.1_1.0.0-ga)?
Thanks for your help,
Aaron
解決済! 解決策の投稿を見る。
Hi Aaron
sabre ai image will not work on sabre sd board as these two boards are different.
One can check sabre ai dts for can records and make similar changes to sabre sd file.
Best regards
igor
Hi Aaron
seems android flexcan usage may be similar to previous versions, so one can
look at efforts described on
https://community.nxp.com/thread/333623
https://github.com/ryangithub/sunxi-can-driver
https://www.technexion.com/products/system-on-modules/edm/edm-modules/detail/EDM1-CF-IMX6
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for the reply this will come in very handy in the future but the root problem I am having is that 'can0' or 'can1' do not appear in the list of devices when typing 'ifconfig -all'.
How do I add the can devices to the Linux kernel in the freescale Android 7.1.1 release?
Thanks,
Aaron
Hi Igor,
I built the image for saber ai (sabreauto_6q) however this does not appear to work on the sabreSD board.
I am using mfgtools to load the image into emmc (mfgtool2-android-mx6dl-sabresd-emmc.vbs). Did I use the correct configuration?
Thanks,
Aaron
Hi Aaron
sabre ai image will not work on sabre sd board as these two boards are different.
One can check sabre ai dts for can records and make similar changes to sabre sd file.
Best regards
igor