FlexCAN gpio selection -- I-MX6 Solo Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexCAN gpio selection -- I-MX6 Solo Controller

1,898 Views
keesjurgen
Contributor I

Hi,

Previously i have used MCF521x controller & there i use to select the GPIO to activate CAN bus Pins of Flexcan in this way.

#define FLEXCAN_GPIO_INIT()   MCF_GPIO_PUCPAR = 0 | MCF_GPIO_PUCPAR_URXD2_CANRX | MCF_GPIO_PUCPAR_UTXD2_CANTX;

Do we have to Activate CAN Bus pins in I-max6 solo controller also ?

I am JUst going through the DataSheet for the Imax6 Solo processor.

i.MX6 Solo Reference Manual


And found that there is multiplexing for CAN1 TX/RX pins. On Page -315 it tells about FLEXCAN1_RX & FLEXCAN1_TX pins Multiplexing.

Also tells how to activate these PIN.


For  CAN_1 transmit pin, FLEXCAN1_TX, there are three PADS :----


Pads(Pins)                                                    Registers

GPIO_7 (ALT3)                      IOMUXC_SW_MUX_CTL_PAD_GPIO07

KEY_COL2 (ALT2)                IOMUXC_SW_MUX_CTL_PAD_KEY_COL2

SD3_CMD (ALT2)                  IOMUXC_SW_MUX_CTL_PAD_SD3_CMD

Now I am having a question how can a single controller FlexCAN_1 can have its TX pin enabled on 3 PADS ?

Does it means :----

Same CAN TX signal CAN be routed to Three different PAD's ?

or I-MAX6 solo comes in 3 different types of controller with diffrent Pads/Pin configuration ?

Any suggestion will be welcomed .

//Kees

Labels (1)
0 Kudos
Reply
1 Reply

1,369 Views
jimmychan
NXP TechSupport
NXP TechSupport

That means you can configure the GPIO_7 to ALT3 which the GPIO_7 pin is used as FLEXCAN1_TX. If GPIO_7 used for other purpose, you can configure the KEY_COL2 to ALT2 which the KEY_COL2 pin is used as FLEXCAN1_TX. If KEY_COL2 used for other purpose, the last choice is set the SD3_CMD to ALT2 for FLEXCAN1_TX.

0 Kudos
Reply