Finding whether the board is C0 silicon

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Finding whether the board is C0 silicon

跳至解决方案
2,180 次查看
jaux_al
Contributor I

I have a iMX8QuadXPlus and I set the machine name to imx8qxpmek but when I tried to boot the board off the SD card that contained the yocto image, nothing shows up. 

I'm currently trying out imx8qxpc0mek to see if it works but how else do you determine if your machine is C0 silicon?

0 项奖励
回复
1 解答
2,095 次查看
igorpadykov
NXP Employee
NXP Employee

also one can look at uboot log

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
12 回复数
1,589 次查看
_angelo_
Contributor III

Om MEK board,

removed the heatsink CPU has a suffix B at the end of the code

 

CPU PCB BLACK 2017 is b0
CPU PCB GREEN 2018 is c0

0 项奖励
回复
2,164 次查看
jaux_al
Contributor I

But I'm not really migrating from B0 to C0. Just want to understand whether my board is C0 silicon or B0

0 项奖励
回复
2,159 次查看
igorpadykov
NXP Employee
NXP Employee

rev.C0 has suffix "C" of processor marking.

 

Best regards
igor

0 项奖励
回复
2,149 次查看
jaux_al
Contributor I

where can I find that on the EVB board though?

0 项奖励
回复
2,144 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复
2,118 次查看
jaux_al
Contributor I

where it does talk about C0 or B0 silicon? I am just trying to get the machine name of my EVB. 

0 项奖励
回复
2,103 次查看
igorpadykov
NXP Employee
NXP Employee

>where it does talk about C0 or B0 silicon?

 

please locate processor on board and look at its marking.

 

Best regards
igor

0 项奖励
回复
2,100 次查看
jaux_al
Contributor I

the only text I see is IMX8-QXP CPU. It has a fan on it so maybe the complete name is hidden underneath, hence my concern about finding the full machine name including the silicon 

0 项奖励
回复
2,096 次查看
igorpadykov
NXP Employee
NXP Employee

also one can look at uboot log

 

Best regards
igor

0 项奖励
回复
2,091 次查看
jaux_al
Contributor I

i have been having issues loading up the yocto image off the SD card. Do you have a sample image of the boot log indicating the silicon type?

0 项奖励
回复
2,170 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jaux_al

 

one can look at AN12770  i.MX 8X C0 Migration Guide Migrating from i.MX 8X B0 to i.MX 8X C0

in particular sect.2.3 Software changes.

 

Best regards
igor

0 项奖励
回复
2,156 次查看
jaux_al
Contributor I

But I'm not looking to migrate between C0 and B0 - just need to know to determine whether my board is C0 or B0

0 项奖励
回复