Hi all,
I'm using Linux+QT for my OS system and using fsl_image_qt5 for my root file system.
I'm trying to transfer file via BT to my iPhone.
So far, I had connected my phone by using bluetoothctl and paired it.
After some googling I decide to using obexctl to transfer my file.
But when I running this command "./usr/lib/bluez5/bluetooth/obexd &" and will give this error for me.
Using X11 for dbus-daemon autolaunch was disabled at compile time, set your DBUS_SESSION_BUS_ADDRESS instead
Is that mean I can't using it without X11?
How can I solve this problem?
Besides, when I running "obexctl" for connecting my iPhone by using this command "connect xx:xx:xx:xx:xx:xx".
P.S. xx:xx:xx:xx:xx:xx is my iPhone BT address.
Then it will give me the error like below.
Client proxy not available
What does this mean?
And how to in solving this?
Thanks in advanced!
Hi ,
I am facing similar issue . how you resolved these ?
You can set DBUS_SESSION_BUS_ADDRESS variable prior running obexd.
It can be performet with the connamd like this:
# export $(dbus-launch)
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
New updated, I've got this information by using bluetoothctl.
[ Bluetooth ]# info 70:81:EB:76:6E:D3
Device 70:81:EB:76:6E:D3
Name: iPhone
Alias: iPhone
Class: 0x7a020c
Icon: phone
Paired: yes
Trusted: yes
Blocked: no
Connected: yes
LegacyPairing: no
UUID: Vendor specific (00000000-deca-fade-deca-deafdecacafe)
UUID: Service Discovery Serve.. (00001000-0000-1000-8000-00805f9b34fb)
UUID: Audio Source (0000110a-0000-1000-8000-00805f9b34fb)
UUID: A/V Remote Control Target (0000110c-0000-1000-8000-00805f9b34fb)
UUID: A/V Remote Control (0000110e-0000-1000-8000-00805f9b34fb)
UUID: NAP (00001116-0000-1000-8000-00805f9b34fb)
UUID: Handsfree Audio Gateway (0000111f-0000-1000-8000-00805f9b34fb)
UUID: Phonebook Access Server (0000112f-0000-1000-8000-00805f9b34fb)
UUID: Message Access Server (00001132-0000-1000-8000-00805f9b34fb)
UUID: PnP Information (00001200-0000-1000-8000-00805f9b34fb)
Modalias: bluetooth:v004Cp6F01d0A30
And when I try using obexctl to connect "Message Access Server" and will show the error like below.
[obex]# connect 70:81:EB:76:6E:D3 00001132-0000-1000-8000-00805f9b34f
b
Attempting to connect to 70:81:EB:76:6E:D3
[obex]#
Failed to connect: org.bluez.obex.Error.Failed
And if i try to connect "Phonebook Access Server", it will connect successfully.
Why I can't connect "Message Access Server"?
By the way, how to send the file to my phone?
When I trying to "ls" then it will show this error to me.
Failed to List: org.bluez.obex.Error.Forbidden
Is that mean i can't list the content?
Thanks in advanced!
Thanks but now I get another problem.
I trying to run obexctl it works great.
But when I trying to connect my iPhone by running "connect xx:xx:xx:xx:xx:xx <UUID>".
It shows me the following error.
[obex]# connect 70:81:EB:76:6E:D3 00001132-0000-1000-8000-00805f9b34f
b
Attempting to connect to 70:81:EB:76:6E:D3
[obex]#
Failed to connect: org.bluez.obex.Error.Failed
"Failed to connect: org.bluez.obex.Error.Failed".
How to solve this problem and why it will show up?
Thanks in advanced!