We're running on IMX8mini, Android9.0, 8G EMMC, flash partition with partition-table-7GB.img, and I can build out the OTA file, update.zip.
And I've verified this .zip file with update_device.py script, to make sure this .zip is not corrupted.
I put this update.zip to the USB stick, and plugin into the device. I checked the UI and the logcat, the system successfully detected this USB stick, and I can browse the files on the USB stick.
But that's all, the system didn't show up the upgrade menu to prompt me to do upgrade, even I waited for hours.
Could anyone give me some tips? As we know, put upgrade.zip to SDcard/USB stick, and plugin into the system, would let system prompt upgrade, which is a standard behavior of Android.
Hi 13614278@qq.com,
To upgrade the OTA package, there are two ways in default BSP.
To follow either of the above methods, please refer to Section 7.2 Implementing OTA update of "Android User's Guide"(attached for your reference).
Regards,
Kunal
Hi 13614278@qq.com,
Are you using Automotive Android or standard Android? If it is Automotive, then SystemUpdater may do what you need.
Regards,
Kunal