Failed to Power Off i.mx6ull board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failed to Power Off i.mx6ull board

1,166 次查看
dhvanil_patel1
Senior Contributor I

HI,

I am working on i.mx6ull based board and I am facing an issue while power off the i.mx6ull board from Linux console.

I am using "imx-4.1-krogoth" branch of "git://git.freescale.com/imx/fsl-arm-yocto-bsp.git" 

root@imx6ullmg:~# poweroff

Broadcast message from root@imx6ullmg (ttymxc0) (Mon Apr 24 08:49:11 2017):
The system is going down for system halt NOW!
INIT: Switching to runlevel: 0
INIT: Sending processes the TERM signal
INIT: Sending processes the KILL signaStopping Dropbear SSH server: stopped /usr/sbin/dropbear (pid 273)
dropbear.
* Stopping Avahi mDNS/DNS-SD Daemon: avahi-daemon
...done.
Stopping advanced power management daemon: no /usr/sbin/apmd found; none killed
apmd.
Stopping domain name service: named.
Stopping system message bus: dbus.
Stopping DHCP server: dhcpd3no /usr/sbin/dhcpd found; none killed
.
Stopping ntpd: done
Error opening /dev/fb0: No such file or directory
Stopping syslogd/klogd: stopped syslogd (pid 315)
stopped klogd (pid 318)
done
Stopping Connection Manager
Stopping Telephony daemon
ALSA: Storing mixer settings...
/usr/sbin/alsactl: save_state:1595: No soundcards found...
Stopping rpcbind daemon...
done.
Stopping Linux NFC daemon
Stopping Lighttpd Web Server: stopped /usr/sbin/lighttpd (pid 341)
lighttpd.
Deconfiguring network interfaces... done.
Stopping radvd: not running.
Sending all processes the TERM signal...
Sending all processes the KILL signal...
random: nonblocking pool is initialized
Unmounting remote filesystems...
Deactivating swap...
Unmounting local filesystems...
EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered
reboot: Power down
Unable to poweroff system

Need help to reslove this issue ASAP.

标签 (4)
标记 (4)
0 项奖励
回复
3 回复数

813 次查看
dhvanil_patel1
Senior Contributor I

Hi igor,

I am using the same source as pointed by above documents. I have also followed the same i.mx6ull evk board. But power off command is not working. 

Need help to find out the root cause.

0 项奖励
回复

813 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

813 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dhvanil

what reference design used for custom board, please try nxp bsp with i.MX6ULL EVK board

linux-imx.git - i.MX Linux Kernel 

Documentation can be found on

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复