Facing issue with porting XEN on IMX8QM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Facing issue with porting XEN on IMX8QM

1,292 次查看
Harish-Sam
Contributor II

Dear,

We are using IMX8QM Evaluation board on that we need to port XEN hypervisor with prebuilt images. 

I have downloaded L4.14.98_2.0.0_ga_images_MX8QMMEK, automotive-10.0.0_2.4.0_image_8qmek2 prebuilt binary setup. 

For porting XEN we following below steps mentioned in i.MX Virtualization User's Guide. 

Steps 

  1. The first FAT partition holds "xen", "Image", and "fsl-imx8qm-mek-dom0.dtb". 
  2. The second and third partitions hold Linux Kernel distributions for Dom0 and DomU. 
  3. Burn imx-boot-imx8qmmek-sd.bin-flash to the SD card offset 32 KB. 

  

In which We have used XEN binary from following folder  

automotive-10.0.0_2.4.0_image_8qmek2. 

  

and we used Image,fsl-imx8qm-mek-dom0.dtb,imx-boot-imx8qmmek-sd.bin-flash binary from following folder 

L4.14.98_2.0.0_ga_images_MX8QMMEK 

  

But we are facing issue with booting, U-Boot image(imx-boot-imx8qmmek-sd.bin-flash) burn on SD card but its not loading. 

Regards,

Harish

标记 (1)
0 项奖励
回复
4 回复数

1,188 次查看
Harish-Sam
Contributor II

Dear Support,

I am using IMX8QM Development board which is designed by Iwave System.

I have successfully built xen Image,Kernel Image,Rootfs and successfully boot up xen but during booting DOM0 kernel processor getting stuck.

Please find attached log and please let me know solution for same.

 

Thanks and Regards,

Harishchandra Samgir

0 项奖励
回复

1,276 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello TCS-Harish,

You are right, you need to take the uboot from a website and modify by yourself if any apply after you burn the SDcard.

Regards

0 项奖励
回复

1,273 次查看
Harish-Sam
Contributor II

Dear Support,

Could you please share me uboot source code.

Thanks you

0 项奖励
回复

1,269 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复