Facing issue in yocto zeus u-boot compilation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Facing issue in yocto zeus u-boot compilation

2,828 次查看
nikhil_sahu2
Contributor III

Hi Experts,

I downloaded and successfully compiled the "core-image-base" for yocto zeus, I am able to compile the standalone kernel with some modification. Similarly when i am able to compile the u-boot even without any modification, I am facing below errors. Kindly help what i am missing or is there any to way to compile standalone u-boot only.

ubuntu@ubuntu:~/zeus/build_sabresd$ bitbake -c cleansstate u-boot-imx
NOTE: Your conf/bblayers.conf has been automatically updated.
Loading cache: 100% |#########################################################################################################################################################################| Time: 0:00:00
Loaded 4067 entries from dependency cache.
ERROR: /home/ubuntu/_zeus/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2019.04.bb: Error executing a python function in <code>: | ETA: --:--:--

The stack trace of python calls that resulted in this exception/failure was:
File: '<code>', lineno: 3, function: <module>
0001:__anon_20__home_ubuntu_zeus_sources_poky_meta_conf_machine_include_arm_feature_arm_thumb_inc(d)
0002:__anon_25__home_ubuntu_zeus_sources_poky_meta_classes_patch_bbclass(d)
*** 0003:__anon_705__home_ubuntu_zeus_sources_poky_meta_classes_base_bbclass(d)
0004:__anon_64__home_ubuntu_zeus_sources_meta_freescale_classes_fsl_dynamic_packagearch_bbclass(d)
0005:__anon_1023__home_ubuntu_zeus_sources_poky_meta_classes_insane_bbclass(d)
0006:__anon_1263__home_ubuntu_zeus_sources_poky_meta_classes_insane_bbclass(d)
0007:__anon_252__home_ubuntu_zeus_sources_poky_meta_classes_package_bbclass(d)
File: '/home/ubuntu/zeus/sources/poky/meta/classes/base.bbclass', lineno: 589, function: __anon_705__home_ubuntu_zeus_sources_poky_meta_classes_base_bbclass
0585:
0586: needsrcrev = False
0587: srcuri = d.getVar('SRC_URI')
0588: for uri in srcuri.split():
*** 0589: (scheme, _ , path) = bb.fetch.decodeurl(uri)[:3]
0590:
0591: # HTTP/FTP use the wget fetcher
0592: if scheme in ("http", "https", "ftp"):
0593: d.appendVarFlag('do_fetch', 'depends', ' wget-native:do_populate_sysroot')
File: '/home/ubuntu/zeus/sources/poky/bitbake/lib/bb/fetch2/__init__.py', lineno: 355, function: decodeurl
0351: """
0352:
0353: m = re.compile('(?P<type>[^:]*)://((?P<user>[^/;]+)@)?(?P<location>[^;]+)(;(?P<parm>.*))?').match(url)
0354: if not m:
*** 0355: raise MalformedUrl(url)
0356:
0357: type = m.group('type')
0358: location = m.group('location')
0359: if not location:
Exception: bb.fetch2.MalformedUrl: The URL: '\' is invalid and cannot be interpreted

ERROR: Failed to parse recipe: /home/ubuntu/zeus/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2019.04.bb

3 回复数

2,620 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Dear Nikhil sahu, 

When you compile for the first time  the u-boot before you use the clean state did it works properly or has failures or crashes?
If you want to compile the u-boot without using yocto you can follow the linux user guide in the part 4.5.11. (How to build U-Boot and Kernel in standalone environment)
You can download that from the next link:https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_LINUX_DOCS
Also please check the  document repository in the next link:https://source.codeaurora.org/external/imx
Hope this might help you.

Do you still have the problem? Or is working properly now?

Regards,
Israel H.

2,620 次查看
nikhil_sahu2
Contributor III

Just adding in original thread, I am using the yocto zeus BSP (imx-5.4.3-1.0.0.xml) below is the url and xml info.

repo init -u https://source.codeaurora.org/external/imx/imx-manifest  -b imx-linux-zeus -m imx-5.4.3-1.0.0.xml

And I am able to compile the "core-image-base" successfully. after that i tried to clean(bitbake -c cleansstate linux-imx) and compile (bitbake  linux-imx) the kernel, i am succeed.

Similarly when i am going to clean the u-boot (bitbake -c cleansstate u-boot-imx), i was facing the above error.

Thanks in advance.

0 项奖励
回复

2,620 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Dear Nikhil sahu,

Did you already solve your problem? Or still need help on this? Please let us know.

Regards,

Israel H.

0 项奖励
回复