Facing difficulty in booting iMX 8M Quad EVK with demo .sdcard image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Facing difficulty in booting iMX 8M Quad EVK with demo .sdcard image

570 次查看
girijapretha
Contributor II

Hi,

I have downloaded the zip file named "L4.9.88_2.0.0_images_MX8MQ" from i.MX 8M Evaluation Kit|NXP. I am trying to boot  the iMX8M QuadEVK using demo images(). I used linux dd command "$ sudo dd if=<image name>.sdcard of=/dev/sdx bs=1M && sync" (given in the Reference Manual) to flash image to the SD card. I have configured all DIP switches as given in Manual. (With the same configuration I am able to boot Android from SD card).

Am I missing any steps to follows ?

Kindly help me to bringup the board

Thanks,

Girija Pretha

标签 (1)
0 项奖励
1 回复

458 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Girija 

one can try with other sd card or using mfg tool, use script

mfgtool2-yocto-mx8-evk-sd2.vbs.

"Manufacturing Toolkit for Linux L4.9.88_2.0.0 i.MX8MQ BSP"

https://www.nxp.com/webapp/Download?colCode=IMX6_L4.9.88_2.0.0_8MQ_MFG_TOOL&appType=license&location... 

Demo Images

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励