FTM in Output compare mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FTM in Output compare mode

1,731 Views
bipin7301
Contributor II

Hi,

[ Environment : Win CE 7 OS on Toradex Colibri iMX7D 512MB board ]

I am using FTM module in output compare mode. I have developed the driver and it is partially working too. But I am not getting the desired result. I have configured FTM in output compare mode with output toggle on channel match. Channel flag sets on channel match however nothing observed on channel output. I am attaching the source code for reference.

Secondly, I want to use an ISR when an event occurs at channel match in(FTM in output compare mode). FTMx_CnSC has a CHIE bit to enable the interrupt so we can enable the interrupt. But how one can trigger a function using this interrupt ? Please guide me, How to write ISR for the channel match interrupt?

Regards

Bipin Kumar

Labels (1)
0 Kudos
Reply
0 Replies