Hi,
I am working BareMetal programming on imx8mmini cortex-a53 processor. I want to know the external GIC distributer which is integrated with cortex-a53 core CPU interface. I need the base address of external GIC distributer and re distributer. I couldn't any information regarding external to the core.
Thanks,
Navaneethan
We suggest you refer the Linux GICv3 driver and dts base address.
Hi,
I am working BareMetal programming. So i am not using the U-boot and Linux. I am using ARM DS-5 startup code and imx-mkimg tool to generate flash.bin. In that startup code they were initializing GIC distributor and Re distributor from base address 0x2f000000. The referred address is right?
In linker script file:
/*
* GICv3 distributor
*/
.gicd 0x2f000000 (NOLOAD):
{
*(.gicd)
}
/*
* GICv3 redistributors
* 128KB for each redistributor in the system
*/
.gicr 0x2f100000 (NOLOAD):
{
*(.gicr)
}
Thanks,
Navaneethan