Hello everyone,
I need to control the 112 pin of the J63 connector, which correspond to the SSP2_SCK. I'm using Linux on my iMX28 (Linux version 4.0.4-fslc+g48548f7).
I know that I just have to find the GPIO_A_B number of my pin and then apply : pin = 32xA + B
But that's the thing, on the hardware schematic datasheet, all pins are adressed that way except the expansion connector ones.
How do I find the pin number of my GPIO ? So I can just run :
echo 1 > /sys/class/gpio/gpioXX/value
To be more specific, I'm using yocto.
Merci!
已解决! 转到解答。
I found it !
I just had to modify the device tree this way : (by adding my pins to the Hog)
ssp2: ssp@80014000 {
compatible = "fsl,imx28-mmc";
bus-width = <8>;
};
pinctrl@80018000 {
pinctrl-names = "default";
pinctrl-0 = <&hog_pins_a>;
hog_pins_a: hog@0 {
reg = <0>;
fsl,pinmux-ids = <
MX28_PAD_SSP2_SCK__GPIO_2_16 /* MY PIN */
MX28_PAD_SSP1_CMD__GPIO_2_13
MX28_PAD_SSP1_DATA3__GPIO_2_15
MX28_PAD_ENET0_RX_CLK__GPIO_4_13
MX28_PAD_SSP1_SCK__GPIO_2_12
MX28_PAD_PWM3__GPIO_3_28
MX28_PAD_LCD_RESET__GPIO_3_30
MX28_PAD_AUART2_RX__GPIO_3_8
MX28_PAD_AUART2_TX__GPIO_3_9
>;
fsl,drive-strength = <MXS_DRIVE_4mA>;
fsl,voltage = <MXS_VOLTAGE_HIGH>;
fsl,pull-up = <MXS_PULL_DISABLE>;
};
Thank you !
Thank you Alejandro for your response.
Well I do know (it's the 80 GPIO), actually I understood my problem, I have to change the defaults configuration of the SSP2_SCK into simple GPIO.
To do that, I need to change the device tree file imx28-evk.dts.
I'm trying this : (don't know if it's gonna work)
ssp2: ssp@80014000 {
compatible = "fsl,imx28-mmc";
pinctrl-names = "default";
pinctrl-0 = <&my_pins_a>;
};
pinctrl@80018000 {
pinctrl-names = "default";
pinctrl-0 = <&hog_pins_a>;
my_pins_a : mypin@0 {
fsl,pinmux-ids = <
MX28_PAD_SSP2_SCK__GPIO_2_16
>;
fsl,drive-strength = <MXS_DRIVE_4mA>;
fsl,voltage = <MXS_VOLTAGE_HIGH>;
fsl,pull-up = <MXS_PULL_DISABLE>;
};
But right now, my biggest problem is how to make yocto generate a new kernel everytime I change the imx28-evk.dts file...
By the way, I bought a Flash memory and I plugged it on the Nand Flash Socket, and I don't know how to put my linux on it ! I'm using a SD card and I simply use :
sudo dd if=imx28-vulog-image-imx28evk.sdcard of=/dev/sdb
So wether I'll have to install U-boot on the Flash and then use /tftpboot procedure (and I don't know how to do that...), or maybe there's I sudo dd command for the nand flash ?
Thank you
Hi,
I doubt there is need to use yocto to generate the dtb again.
You can try the next from the top source directory:
make ARCH=arm dtbs
it should generate again all the dtbs with the new configuration.
/Alejandro
alejandrolozano:
Hi,
I doubt there is need to use yocto to generate the dtb again.
You can try the next from the top source directory:
make ARCH=arm dtbs
it should generate again all the dtbs with the new configuration.
/Alejandro
But is it gonna change the imx28-vulog-image-imx28evk.sdcard ?
It works ! I simply modified my imx28-evk.dts in "build/tmp/work-shared/imx28evk/kernel-source/arch/arm/boot/dts/imx28-evk.dts"
And then in the build directory I ran :
> > bitbake -c devshell virtual/kernel
> > make dtbs
I found the dtb file in "tmp/work/imx28evk-poky-linux-gnueabi/linux-fslc/4.0+gitAUTOINC+48548f793f-r0/build/arch/arm/boot/dts/imx28-evk.dtb"
After that I made a recipe to copy it in my imx28 in "/usr/bin/" and on the imx I replaced the dtb in "/run/media/mmcblk0p2" by mine. After a reboot, the gpio80 was not configured as spi2_sck anymore !
But the pin still doesn't change. When I run echo 1 > /sys/class/gpio/gpio80/value, the pin is still at 0...
I'm looking into my dts... any idea ? I replaced the "compatible = "fsl,imx28-mmc""; by "compatible = "fsl,imx28-gpio";" but still nothing...
I found it !
I just had to modify the device tree this way : (by adding my pins to the Hog)
ssp2: ssp@80014000 {
compatible = "fsl,imx28-mmc";
bus-width = <8>;
};
pinctrl@80018000 {
pinctrl-names = "default";
pinctrl-0 = <&hog_pins_a>;
hog_pins_a: hog@0 {
reg = <0>;
fsl,pinmux-ids = <
MX28_PAD_SSP2_SCK__GPIO_2_16 /* MY PIN */
MX28_PAD_SSP1_CMD__GPIO_2_13
MX28_PAD_SSP1_DATA3__GPIO_2_15
MX28_PAD_ENET0_RX_CLK__GPIO_4_13
MX28_PAD_SSP1_SCK__GPIO_2_12
MX28_PAD_PWM3__GPIO_3_28
MX28_PAD_LCD_RESET__GPIO_3_30
MX28_PAD_AUART2_RX__GPIO_3_8
MX28_PAD_AUART2_TX__GPIO_3_9
>;
fsl,drive-strength = <MXS_DRIVE_4mA>;
fsl,voltage = <MXS_VOLTAGE_HIGH>;
fsl,pull-up = <MXS_PULL_DISABLE>;
};
Thank you !