Ever run imx6D with a single 16-bit DDR3 device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ever run imx6D with a single 16-bit DDR3 device?

ソリューションへジャンプ
623件の閲覧回数
EdSutter
Senior Contributor II

I may have need to run my iMX6D based hardware with only the lowest 16-bit device active on the data bus.

To confirm that this is possible, I'm trying to configure my sabresd board in that mode.

I thought all I had to do was change the DSIZ bits in the MMDCx_MDCTL register

(part of DCD data) to 00.  When I do that (in u-boot), I am then not able to do a USB-based download.

Is there something else that needs to be changed?

Ed

ラベル(1)
0 件の賞賛
1 解決策
501件の閲覧回数
EdSutter
Senior Contributor II

Ok, I'm self-answering this...

Musta had something confused when I first tried this (above); because now I am running with an iMX6D-based board that has only one 16-bit DDR3 device on the bus and all I did was change the DSIZ bits in MMCDx_MDCTL (0x021b0000) from 0x831a0000 to 0x83180000 to make that happen.

元の投稿で解決策を見る

0 件の賞賛
1 返信
502件の閲覧回数
EdSutter
Senior Contributor II

Ok, I'm self-answering this...

Musta had something confused when I first tried this (above); because now I am running with an iMX6D-based board that has only one 16-bit DDR3 device on the bus and all I did was change the DSIZ bits in MMCDx_MDCTL (0x021b0000) from 0x831a0000 to 0x83180000 to make that happen.

0 件の賞賛