Ethernet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet

522 次查看
saida
Contributor II

hi i.mx6 community

i have sabresd board duallite

im my custom board i have ethenet phy dp83848 and magnetic is hx1148. and i am configuring transceiver in MII10 mode in u-boot-2015.01 and  also configured related IO MUX PADS

now i set ipaddr, serverip and ethaddr environment variables in u-boot. this mac is from my sabresd board.

now when i do  #ping serverip

i am getting this error

ARP Retry count exceded : starting again

i am able to read mii registers and the same procedure as i mentioned above is working for sabresd board

so what could be the error, or if i am doing any mistake please help me in this regard or is there any hardware problem ? (my chassis ground is in floating)

please any one can help in this regard so that my custom board will the OK with all my required peripherals

thank you

SAIDA

标签 (1)
0 项奖励
回复
2 回复数

384 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Saida S,

I would recommend reviewing the software configuration. Since you are using a different PHY than the SABRE board you would need to change the U-Boot configuration and Driver in order to accommodate the new PHY. There is some information on the driver configuration on the manufacturer’s website.

Regards,

0 项奖励
回复

384 次查看
saida
Contributor II

hi

thank you

i sorted out the problem

regards

saida

0 项奖励
回复