Ethernet not found on iMX8M Mini EVK board with latest i3D SDK sdcard image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet not found on iMX8M Mini EVK board with latest i3D SDK sdcard image

Jump to solution
1,373 Views
robiwan
Contributor II

Trying to get the latest i3D SDK up and running on my iMX8M Mini EVK board (https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-...), and I get the following u-boot log:

U-Boot SPL 2020.04-5.4.70-2.3.0+ge5f6ae61aa (May 29 2021 - 02:56:43 +0000)
power_bd71837_init
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1
NOTICE: BL31: v2.2(release):rel_imx_5.4.70_2.3.0-0-gf1d7187f2
NOTICE: BL31: Built : 10:18:19, Feb 10 2021


U-Boot 2020.04-5.4.70-2.3.0+ge5f6ae61aa (May 29 2021 - 02:56:43 +0000)

CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 41C
Reset cause: POR
Model: NXP i.MX8MM Audio board 2.0
DRAM: 2 GiB
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... Run CMD11 1.8V switch
*** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial

BuildInfo:
- ATF f1d7187
- U-Boot 2020.04-5.4.70-2.3.0+ge5f6ae61aa

Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
Net: Could not get PHY for FEC0: addr 0
Could not get PHY for FEC0: addr 0
No ethernet found.

Normal Boot
Hit any key to stop autoboot: 0

As can be seen, ethernet phy is not found. 

Any ideas?

A previous version of the SDK works fine.

Labels (1)
0 Kudos
1 Solution
1,291 Views
robiwan
Contributor II

Ok, my i3D contact at NXP has confirmed that the AB2 board is needed for the i3D image. We have such a board inbound, so should fix the problem.

View solution in original post

0 Kudos
9 Replies
1,346 Views
robiwan
Contributor II

Sorry, title was wrong. I've edited it now. It is the iMX8M Mini EVK board I have: https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-...

Although, upon closer inspection, the CPU board I have doesn't look the same, it is smaller. DSC_0005.JPG

0 Kudos
1,334 Views
robiwan
Contributor II

I downloaded the other one you posted (L5.4.70-2.3.0_images_MX8MMEVK), which image file should I try? The imx-image-full-imx8mmevk.tar.bz2 one?

0 Kudos
1,331 Views
igorpadykov
NXP Employee
NXP Employee

one can try to follow sect.4.3.2 Copying the full SD card image Linux Guide included in

Documentation

 

Best regards
igor

 

 

 

0 Kudos
1,323 Views
robiwan
Contributor II

Ok, with imx-image-full-imx8mmevk.wic, ethernet works. But there is no Immersive 3D components, and I need to setup the EVK with i3D in order to support a customer.

0 Kudos
1,312 Views
igorpadykov
NXP Employee
NXP Employee

unfortunately Immersiv3D is not supported here, for support of this software please apply to

local NXP sales.

 

Best regards
igor

0 Kudos
1,292 Views
robiwan
Contributor II

Ok, my i3D contact at NXP has confirmed that the AB2 board is needed for the i3D image. We have such a board inbound, so should fix the problem.

0 Kudos
1,358 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robert

 

>Trying to get the latest i3D SDK up and running on my iMX8M EVK board

 

from log "CPU: i.MX8MMQ" seems this i.MX8M Mini EVK, not iMX8M EVK (with i.MX8MQ processor)

so images for i.MX8M Mini EVK should be used    i.MX 8M Mini EVK

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos
1,345 Views
robiwan
Contributor II

Thanks, I'll try that image!

0 Kudos