Hello NXP TechSupport
i'm using i.MX 8M Nano EVK + BD71837 (PMIC).
facing error while compiling Linux BSP.
# Versions
1] Linux 4.14.98_2.3.0
2] Linux 4.14.98_2.2.0 for i.MX 8M Nano GA
# Errors
ERROR: arm-compute-library-18.11+gitAUTOINC+64441b79b8-r0 do_unpack: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-V9zMsPBnLC"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/sources/poky/scripts:/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot/usr/bin/crossscripts:/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/usr/sbin:/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/usr/bin:/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/sbin:/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/bin:/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/sources/poky/bitbake/bin:/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/build-xwayland/tmp/hosttools"; export HOME="/home/nikhil"; git -c core.fsyncobjectfiles=0 checkout -B imx_18.11 64441b79b83e0790008486779054e9da891537f3 failed with exit code 128, output:
git-lfs smudge -- 'data/images/1280x720.ppm': 1: git-lfs smudge -- 'data/images/1280x720.ppm': git-lfs: not found
error: external filter git-lfs smudge -- %f failed -1
error: external filter git-lfs smudge -- %f failed
fatal: data/images/1280x720.ppm: smudge filter lfs failed
ERROR: arm-compute-library-18.11+gitAUTOINC+64441b79b8-r0 do_unpack: Function failed: base_do_unpack
ERROR: Logfile of failure stored in: /home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/temp/log.do_unpack.29048
ERROR: Task (/home/nikhil/OLD-Linux-BSP-L4.14.98_2.2.0/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-support/arm-compute-library/arm-compute-library_git-imx.bb:do_unpack) failed with exit code '1
3] Linux 5.4.3_1.0.0
# Error
- Unable to start bitbake server.
4] Linux 5.4.47_2.2.0 [ latest ]
- Successfully compiled but while booting it's showing an error as can't find PMIC:PCA9450.
I'm not understanding which Linux BSP I should use which will compiled successfully and boot successfully too.
Please share resulting solution.
Thanks
Nikhil
Linux 4.14.98_2.3.0 is available for 8m nano, what's your build steps? I can build it successfully, but I used ubuntu 18.04, refer to your error message, it seems that this is network issue, try to remove and build again, like bitbake -c cleansstae xx and bitback -c xx