Error message of mx515

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error message of mx515

579件の閲覧回数
RobbieJiang
Contributor IV

Hi,

Sometimes  I got the following error message when starting a gstreamer pipeline with mfw_v4lsrc,

or during the running of the gstreamer pipeline ( mfw_v4lsrc->mfw_vpuencoder->h264pay->udpsink)

ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received

ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_5 = 0x00100000

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x01000000

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_10 = 0x02000000

ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received

ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_5 = 0x00100000

mxc_ipu mxc_ipu: handler already installed on irq 451

mxc_ipu mxc_ipu: DC irq 451 in use

What's the exact meaning of these error message?

Does it matter?

Or can I just ignore them?

Regards,

Robbie

ラベル(3)
0 件の賞賛
0 返答(返信)