i am using Android 10 BSP
i am running on my image built
As i wanted to export GPIO88 in the device tree
pinctrl-0 = <&pinctrl_hog_1>;
pinctrl_hog_1: hoggrp-1{
fsl,pins = <
MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41
>;
};
and buiit only boot.img file
image built without any error
Boot image for i.MX 8M Mini EVK LPDDR4 board
source build/envsetup.sh
lunch evk_8mm-userdebug
./imx-make.sh bootimage -j4
then used to partition an SD Card
sudo ${MY_ANDROID}/device/nxp/common/tools/imx-sdcard-partition.sh -f <soc_name> /dev/sdX
flashing to SD card was finish without error
then connected imx8mm in putty or minicon for debug
i have attached the log below