I have the same issue.
My Board is i.MX 8M Mini EVKB.
And MY BSP is Android Q10.0.0_2.6.0 (Linux 5.4.70 kernel).
Which version of BSP are you using?
Are you running the demo image? or running the image you built?
Could you tell me more details about your issue?
i am using Android 10 BSP
i am running on my image built
As i wanted to export GPIO88 in the device tree
pinctrl-0 = <&pinctrl_hog_1>;
pinctrl_hog_1: hoggrp-1{
fsl,pins = <
MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41
>;
};
and buiit only boot.img file
image built without any error
Boot image for i.MX 8M Mini EVK LPDDR4 board
source build/envsetup.sh
lunch evk_8mm-userdebug
./imx-make.sh bootimage -j4
then used to partition an SD Card
sudo ${MY_ANDROID}/device/nxp/common/tools/imx-sdcard-partition.sh -f <soc_name> /dev/sdX
flashing to SD card was finish without error
then connected imx8mm in putty or minicon for debug
i have attached the log below