Hello,
I want to read a memory stick plugged in to the OTG port of my custom i.MX6 board. On the board the USB_OTG_PWR is configured as KEY_ROW4(ALT2). When I use "usb start" command I see the EHCI controller initialized but no storage device found. So, my questions:
1) Does the usb driver enable VBUS power automatically or I need to enable it manually? If yes then how do I do that? Which register controls this signal?
2) Does the state of the OTG_ID signal affect the functionality?
Thanks,
Vitaly
regarding GPIO, linux driver has more capabilites and supports
"otg" mode and HNP as described for example in
sect.39.3.11 USB OTG HNP and SRP Support Documentation
Best regards
igor