Enabling MIPI DSI interface on freescale Yocto build

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enabling MIPI DSI interface on freescale Yocto build

1,626 次查看
epicedium
Contributor II

What are the steps to enable and configure MIPI DSI on freescale's yocto platform? I'm using a Variscite iMX.6 board and have been developing with the LVDS interface. Connecting a TFT to the MIPI DSI is giving me nothing, and I'm struggling to find documentation for;

- Is the MIPI DSI enabled in the kernel? Is there a driver?

- If so... What config files do I create or enable, to configure the interface?

Thanks!

标签 (4)
0 项奖励
1 回复

1,093 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kris

please refer to Linux documentation (Linux Manual, MIPI DSI Chapter ) on

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励