Hi,
In the i.MX_Linux_Release_Notes.pdf I come across this statements:
I found the zImage-imx6ul-14x14-evk-csi.dtb in the Mfgtools.
1) Can the 'zImage-imx6ul-14x14-evk-csi.dtb' found in Mfgtools be used to enable CSI support for V4L2 on i.MX6UL EVK? If yes, I just need to modify the 'ucl2.xml' file to burn this dtb file to the target or any other steps needed?
2) If I want to build my own dtb, how can one make changes to the kernel source to enable CSI support?
Thanks.
Hi Alan
1. yes
2. one can look at Chapter 19 OmniVision Camera Driver attached Linux Manual.
and 0v5640 entries in imx6ul-14x14-evk.dts.imx6ul-14x14-evk-csi.dts
linux-2.6-imx.git - Freescale i.MX Linux Tree
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------