Hi all,
Do you know if it is possible to enable Jumbo Frames on iMX8QM, and if yes, how could I do that?
The Atheros AR8031-al1b datasheet says that it supports Jumbo Frame up to 10 kB https://www.application-datasheet.com/pdf/qualcomm/ar8031-al1b.pdf
But executing "ip -d link list" maxmtu is 1966 byte
On the iMX8MPlus documentation (11.7.6.1.2.3) I read that the ENET_QOS memory map has a register, MAC Configuration Register, which has a bit (bit 16, JE) that have to be asserted to enable Jumbo Frames. Do you know if iMX8QM has something similar? How I suppose to assert that bit eventually?
Thanks,
Vincenzo
Hi, thank you for your reply.
Do you know whether I have to modify the if_ether.h file and build it again or I just have to modify the file?
Unfortunately the latter didn't work for me.