Enable MIPI display on i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable MIPI display on i.MX6DL

Jump to solution
1,852 Views
tonioch
Contributor III

Hello everyone,

I'm trying to enable the MIPI display (DSI) on my board and I've encountered some problems.

I tried to modify the file imx6qdl-sabresd.dtsi and set the status of mxcfb3 and lcd to okay but it didn't work neither:

mxcfb3: fb@2 {

        compatible = "fsl,mxc_sdc_fb";

        disp_dev = "lcd";

        interface_pix_fmt = "RGB565";

        mode_str ="CLAA-WVGA";

        default_bpp = <16>;

        int_clk = <0>;

        late_init = <0>;

        status = "okay";

    };

lcd@0 {

        compatible = "fsl,lcd";

        ipu_id = <0>;

        disp_id = <0>;

        default_ifmt = "RGB565";

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_ipu1_1>;

        status = "okay";

    };

I've got the following message when I'm booting the card with the image core-image-minimal:

mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed

MIPI DSI driver module loaded

mxc_sdc_fb fb.32: register mxc display driver lcd

mxc_sdc_fb fb.32: ipu0-di0 already in use

mxc_sdc_fb: probe of fb.32 failed with error -16

I've also tried to change the disp_id of "&mipi_dsi" without success.

Anybody knows how to solve this?

Regards,

Antoine

0 Kudos
Reply
1 Solution
622 Views
tonioch
Contributor III

I've found the answer, to enable the MIPI display, you have to disable the ldb display and change the disp_id and framebuffer of mipi_dsi on the imx6qdl-sabresd.dtsi file:

Here's my configuration in order to enable the mipi display, hope that will help you.

mxcfb1: fb@0 {

        compatible = "fsl,mxc_sdc_fb";

        disp_dev = "mipi_dsi";

        interface_pix_fmt = "RGB565";

        mode_str ="TRULY-WVGA";

        default_bpp = <16>;

        int_clk = <0>;

        late_init = <0>;

        status = "okay";

    };

lcd@0 {

        compatible = "fsl,lcd";

        ipu_id = <1>;

        disp_id = <1>;

        default_ifmt = "RGB565";

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_ipu1_1>;

        status = "okay";

    };

&ldb {

          ipu_id = <1>;

          disp_id = <1>;

          ext_ref = <1>;

          mode = "sep1";

          sec_ipu_id = <1>;

          sec_disp_id = <0>;

          status = "disabled";

}

&mipi_dsi {

    dev_id = <0>;

    disp_id = <1>;  /* modif */

    lcd_panel = "TRULY-WVGA";

    disp-power-on-supply = <&reg_mipi_dsi_pwr_on>;

    resets = <&mipi_dsi_reset>;

    status = "okay";

};

View solution in original post

0 Kudos
Reply
1 Reply
623 Views
tonioch
Contributor III

I've found the answer, to enable the MIPI display, you have to disable the ldb display and change the disp_id and framebuffer of mipi_dsi on the imx6qdl-sabresd.dtsi file:

Here's my configuration in order to enable the mipi display, hope that will help you.

mxcfb1: fb@0 {

        compatible = "fsl,mxc_sdc_fb";

        disp_dev = "mipi_dsi";

        interface_pix_fmt = "RGB565";

        mode_str ="TRULY-WVGA";

        default_bpp = <16>;

        int_clk = <0>;

        late_init = <0>;

        status = "okay";

    };

lcd@0 {

        compatible = "fsl,lcd";

        ipu_id = <1>;

        disp_id = <1>;

        default_ifmt = "RGB565";

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_ipu1_1>;

        status = "okay";

    };

&ldb {

          ipu_id = <1>;

          disp_id = <1>;

          ext_ref = <1>;

          mode = "sep1";

          sec_ipu_id = <1>;

          sec_disp_id = <0>;

          status = "disabled";

}

&mipi_dsi {

    dev_id = <0>;

    disp_id = <1>;  /* modif */

    lcd_panel = "TRULY-WVGA";

    disp-power-on-supply = <&reg_mipi_dsi_pwr_on>;

    resets = <&mipi_dsi_reset>;

    status = "okay";

};

0 Kudos
Reply