Hello,
I would like display standard demo on display FRD55 using standard code form emcraft repository (https://www.emcraft.com/som/imx-8m/using-mipi-dsi-to-connect-the-frd-55-display-panel).
After the system boots up display is dark, nothing show (backlight work). I check hardware and every power supply is fine. In logs I have the same information like in tutorial (see in attachment).
I checked frame buffer set and timings have only 0 value. Is it correct ? Below is data from terminal:
root@imx8m-som:~# fbset
mode "1920x1080"
geometry 1920 1080 1920 1080 32
timings 0 0 0 0 0 0 0
accel true
rgba 8/16,8/8,8/0,0/0
endmode
I tried run lcdtest but effect is the same: display is dark. Below is data from terminal:
root@imx8m-som:~# lcdtest
1920x1080, 32bpp
The framebuffer can be accessed at the address 0xffffa3851000
I tried upload frame buffer random data but I got receive, that buffor didn’t left space:
root@imx8m-som:~# > sudo cat /dev/urandom > /dev/fb0
cat: write error: No space left on device
Please give me some advice what is wrong,
Hi Mateusz
one can reflash image using prebuilt images of build own using emcraft resources
i.MX 8M System-On-Module Resource Directory
Please note that this board is not supported by nxp and one can apply
to emcraft support: Services
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------