There is the following statement on page 13 of the "IMX7DS_3N09P( Rev. 1.2, 3/2023)".
Assert RX_EQS, RX_EQ_SEL by writing data “0x48” to the register address 0x306d0090.
I think the register address is 0x306d0060, is that correct?
There is no explanation about 0x306d0090 in "i.MX 7Dual Applications Processor Reference Manual (Rev. 1, 01/2018)"
I think it's probably PCIE_PHY_TRSV_REG24. (p.3757).
The register address of PCIE_PHY_TRSV_REG24 is stated as 306D_0000h base + 96h offset = 306D_0096h.
And I think the address is 0x306d0060.
See page below
Sincerely,
mio
解決済! 解決策の投稿を見る。
Dear @mio ,
PCIE_PHY_TRSV_REG24, 24 is HEX, convert it to DEC, it is PCIE_PHY_TRSV_REG(2x16+4) = PCIE_PHY_TRSV_REG36.
offset address is 36x4=144D, convert it to HEX, offset address is 0x90.
So PCIE_PHY_TRSV_REG24 address is "306D_0000h base + 0x90 offset" = 0x306D0090h.
So in IMX7DS_3N09P, the address is no problem, But in datasheet, offset is not correct.
Thanks!
Regards,
weidong
Dear @mio ,
PCIE_PHY_TRSV_REG24, 24 is HEX, convert it to DEC, it is PCIE_PHY_TRSV_REG(2x16+4) = PCIE_PHY_TRSV_REG36.
offset address is 36x4=144D, convert it to HEX, offset address is 0x90.
So PCIE_PHY_TRSV_REG24 address is "306D_0000h base + 0x90 offset" = 0x306D0090h.
So in IMX7DS_3N09P, the address is no problem, But in datasheet, offset is not correct.
Thanks!
Regards,
weidong